This step establishes a connection between the PC running Latte and the TRF1208-AFE7950-EVM.
- In the scripts window, select setup.py and press F5 to run the program.
- Check the Log window to ensure there are no errors where the following line
should be displayed four times: Kintex RegProgrammer – USB Instrument created.
- Missing or obsolete drivers for the FT4232H chip in the TRF1208-AFE7950-EVM is a common error source. Use the device manager to verify a connection between the PC and the EVM by checking the USB instantiations.
- Update the PC with the appropriate driver, if necessary.