SBAU392A July 2022 – January 2023 AFE7950 , TRF1208
Figure 3-1 shows how the Latte UI is split into 8 windows (labeled 1 to 8) with the functionality that follows:
This window (also called Scripts) shows the list of python scripts available that generate the register commands to configure the TRF1208-AFE7950-EVM. The script files shown are located in the ..\Documents\Texas Instruments\Latte\projects\AFE79xx\bring-up folder. Modify and create new scripts as necessary, which appear in this sub-window when Latte is restarted.
This window (also called Editor) shows the code in the script currently selected and can be used to modify and save the code as necessary.
These windows get updated as the scripts run to configure the TRF1208-AFE7950-EVM, and are mostly informational.
This window (also called Command Line) is used to enter and run individual commands. Examples of such commands include changing the TX, RX, FBRX DSA, NCOs, and so forth.
This window (also called Log) displays messages during execution of scripts to display the current status. This window is also used for troubleshooting.