SBOA345 June   2021 ADC10D1000QML-SP , ADC12D1600QML-SP , ADC12D1620QML-SP , INA1620 , OPA132 , OPA134 , OPA1602 , OPA1604 , OPA1611 , OPA1612 , OPA1622 , OPA1632 , OPA1637 , OPA1641 , OPA1642 , OPA1644 , OPA1652 , OPA1654 , OPA1655 , OPA1656 , OPA1662 , OPA1664 , OPA1671 , OPA1677 , OPA1678 , OPA1679 , OPA1688 , OPA1692 , OPA2132 , OPA2134 , OPA4132 , OPA4134

 

  1.   Trademarks
  2. 1Thermal Noise
  3. 2Operational Amplifier Voltage Noise
    1. 2.1 Flicker Noise
    2. 2.2 Broadband Noise
  4. 3Operational Amplifier Current Noise
    1. 3.1 Taking a Deeper Look at Noise Sources
  5. 4Calculating Voltage Noise at the Output
  6. 5Summary

Thermal Noise

Resistors can be a major contribution to the overall noise of an audio circuit. The noise generated from a resistor, also known as thermal noise, is noise generated by the random motion of charges within the resistor. We can calculate the noise generated by an ideal resistor using Equation 1.

Equation 1. GUID-20200605-SS0I-THQ0-QNLV-LLXTD3J8WNFG-low.gif

Where

  • en(R) = Noise spectral density from resistance in nV/√Hz
  • k = Boltzmann’s constant 1.38 x 10-23 J/K
  • Tk = Temperature in Kelvin
  • R = The input resistance referred to the non-inverting terminal of the amplifier
GUID-20200605-SS0I-1W24-CT7Q-7KHKBXKBMQQV-low.gifFigure 1-1 Voltage Noise Density Curve

Figure 1-1 displays the relationship between noise spectral density (in nV/√Hz) and resistance (in ohms) plotted for T = 25°C (298K) with varying source resistance values. At just 1k ohms of source resistance the voltage noise is already at 4nV/√Hz.

It’s important to note that an ideal resistor will exhibit predictable noise density that is flat across the frequency spectrum. Multiplying Equation 1 by the noise bandwidth yields RMS. The noise bandwidth is the bandwidth of your circuit. This bandwidth can either be set by the operational amplifier internal circuitry or by using a filter. This RMS noise calculation is shown in Equation 2.

Equation 2. GUID-20210120-CA0I-5TQ2-CCKC-KDN3VQ2GQXRQ-low.gif