SBOA589 May 2024 INA849 , JFE2140
Sensors with a high source impedance can be purely resistive, capacitive, inductive or a combination of the three. High source impedance sensors that produce small signals on the order of a few thousandths of a volt often require amplfication from a low noise and high input impedance pre-amplifier. Amplifiers with bipolar junction transistor (BJT) input stages are popular for the low voltage noise characteristics. BJT devices typically have higher current noise compared to the complementary metal-oxide semiconductor (CMOS)-input and junction field-effect transistor (JFET)-input counterparts. When paired with high source impedance sensors, the current noise from BJT input stages translates into an increase of additional voltage noise. Using a complementary metal-oxide semiconductor (CMOS) device is a good choice for a high input impedance; however, the noise performance is worse than that of a bipolar input. The discrete junction field-effect transistor (JFET) has better 1/f noise performance than the CMOS device and also has high input impedance. More details are found in the Trade-offs Between CMOS, JFET, and Bipolar Input Stage Technology application report. This application brief discusses how to interface high source impedance sensors with high current noise BJT instrumentation amplifiers using discrete matched JFETs. Two preamplifier topologies are compared in this application brief with analysis of trade-offs and how to decide when to use one topology over the other.
Figure 1 shows a preamplifier topology using the INA849. The INA849 is biased with a single supply of 12V. The OPA145 outputs a mid-supply DC voltage of 6V and drives the reference pin Ref and the input common mode voltage of the INA849. The INA849 has a BJT input stage with ultra low voltage noise. BJT input stages are popular choices for the low voltage noise characteristics. When paired with high source impedance sensors the current noise from BJT input stages translates into an additional voltage noise.
A discrete JFET such as TI's JFE2140, when followed by a bipolar instrumentation amplifier such as the INA849, offers a way to achieve high input impedance and low noise with flexible biasing, see Figure 2. The JFETs Q1A and Q1B are each configured in a source follower configuration and replace the front end of the INA849. The INA849 is configured in a gain of 60dB. Source impedances Rsource1 and Rsource2 are now connected to the high input impedance and low current noise discrete JFET front end. The discrete JFET and INA preamplifier circuit offers the low input current noise of the JFETs and the low voltage noise of the INA.
Figure 3 shows noise performance comparisons between the two preamplifier topologies shown in Figure 1 and Figure 2 with various source impedances Rsource. With low source impedance sensors the INA849 outperforms the JFET design. As Rsource increases the preamplifier shown in Figure 2 outperforms the INA849 alone.
Table 1 shows the total circuit current consumption and noise tradeoffs between the two preamplifier topologies. The total current consumption from the design shown in Figure 1 is 6.71mA. The total current consumption of the JFET front end design shown in Figure 2 is 9.88mA. This represents a 47.2% increase in total current consumption. The addition of the discrete JFETs improves the noise performance by reducing the input referred broadband noise by -64.4% when using a source impedance of Rsource = 100kΩ. Figure 3 shows the improvement in the noise when using the JFET + INA849 topology paired with high source impedances.
Preamplifier Topology | Total Iq (mA) | Percent Increase in Iq | Total Voltage Noise
Input Referred f = 1kHz |
Percent Decrease in Voltage Noise |
INA849 | 6.71 | - | 162.07 | - |
JFET + INA849 | 9.88 | 47.2% | 57.63 | -64.4% |
When deciding to use one of the two topologies shown in Figure 1 and Figure 2 a simple calculation is used. In general if the use of the JFET input devices results in lower noise. Additional detail can be found in the application note Impact of Current Noise in CMOS and JFET Amplifiers. The INA849 has a typical current noise specification of .
When Rsource = 13.6kΩ, Table 2 shows that enR = eni_INA = 21.16 (nV/√Hz). Following this guidance there is a improvement in noise when using the discrete JFET and INA preamplifier from Figure 2.
Rsource(Ω) | enR (nV/√Hz) | eni_INA(nV/√Hz) | INA Calculated Total Input Referred Noise en_Total_INA(nV/√Hz) |
JFET + INA Calculated Total Input Referred Noise en_Total_JFET_INA(nV/√Hz) |
---|---|---|---|---|
100 | 1.81 | 0.16 | 2.08 | 2.56 |
500 | 4.06 | 0.78 | 4.25 | 4.44 |
1000 | 5.74 | 1.56 | 6.03 | 6.01 |
1,360 | 6.69 | 2.12 | 7.09 | 6.93 |
5,000 | 12.83 | 7.78 | 15.04 | 12.95 |
10,000 | 18.14 | 15.56 | 23.92 | 18.23 |
13,600 | 21.16 | 21.16 | 29.94 | 21.23 |
50,000 | 40.57 | 77.78 | 87.73 | 40.61 |
The values in Table 2 are calculated using Equation 3 through Equation 6 where the values shown in Table 3 are used.
Value | Description |
---|---|
Boltzmann Constant | |
Temperature in Kelvin | |
Broadband Voltage Noise of JFE2140 Biased at 1.59mA, f = 1kHz | |
Broadband Voltage Noise of INA849 G = 60dB, f = 1kHz | |
Broadband Current Noise of INA849 G = 60dB, f = 1kHz |
The preamplifier topologies have balanced inputs. For this reason a factor is used in Equation 3 and Equation 4.
Discrete JFETs offer bias flexibility by adjusting the drain to source voltage VDS and gate to source voltage VGS. A few key JFET biasing considerations can be made when designing the preamplifier topology shown in Figure 2. Figure 4 shows the drain to source current IDS vs VDS. Bias the JFETs with sufficient VDS to operate in the saturation region.
Figure 5 shows IG vs VDS. Bias VDS such that the gate current is lower than the INA849 bias current.