SBOU302A June 2023 – December 2023 INA740A , INA740B , INA745A , INA745B , INA780A , INA780B
Table 2-1 lists the contents of the EVM kit. Contact Texas Instruments Customer Support if any component is missing.
ITEM | QUANTITY |
---|---|
INA740AEVM, INA740BEVM, INA741EVM, INA745AEVM, INA745BEVM, INA741EVM, INA780AEVM, INA780BEVM, OR INA781EVM test board | 1 |
Note that this EVM requires the TI Sensor Control Board (SCB), which is sold separately.
Currently, there are two versions to the EVMs: version E1 and version A. This is because not all device variants are being fully released at the same time. Version A is functionally and thermally equivalent to E1 except for the following:
Until all devices have been fully released, this document covers both versions.