Use the following guidelines for Noise Figure (NF) measurement:
- As Figure 4-3 shows, the traditional Y-factor method can be used for the NF measurement
using a Noise Diode and a spectrum analyzer (or a Noise Figure Analyzer).
- While doing the measurement, take into account
any RF cable losses to the EVM board. Any external input attenuator added for
matching results in proportional NF degradation and must be calibrated out in
the measurement.
- Also, onboard losses of the input traces at the device input pin must be factored into the NF measurement.
- If the loss after the device output is significant, then note to factor the
output loss into the NF measurement. Use the Friis equation to calculate
the Noise Figure of the device from the total measured NF.