Use the following steps when
connecting the equipment:
- Set the input
power supplies to 6 V (max), and turn the power supplies
off.
- Connect the
positive voltage lead from the input power supply to VIN at
the J1 connector of the EVM.
- Connect the
ground lead from the input power supply to GND at the J6
connector of the EVM.
- Connect a 0-A to
1-A load between VOUT J2 connector and GND J7
connector.
- Disable the
output by shorting VEN to GND through J5.