SCDA008C June 2021 – November 2021 CD4052B , TS3A225E , TS3A44159
A PMOS is similar to an NMOS (see Figure 2-2). However, to keep the source-to-drain resistance low, the difference in the source-to-gate voltage (VSG) should be greater than the threshold voltage. In a PMOS, the terminal with the lowest voltage is considered to be the drain.