SCDA008C June 2021 – November 2021 CD4052B , TS3A225E , TS3A44159
The most basic signal-switch structure is an NMOS pass transistor, with the gate driven by a CMOS inverter. The simplified structure is shown in Figure 3-1.
When the output enable (OE) signal is low, the voltage at the gate is high, or equal to VCC. If the voltage at the drain (VI) is less than VCC by the threshold voltage of the n-channel transistor, the on-state resistance (ron) is low and the voltage at the source is equal to VI (VO = VI). If VI approaches VCC, ron increases rapidly, the source voltage does not increase with the drain voltage, and the output voltage remains at VCC– VT. A limitation of the NMOS series switch is that it can pass signals only up to a threshold voltage below VCC. Figure 3-2 shows the general shape of ron vs VI characteristic of a typical NMOS series switch.