Design Goals
Parameter | Design Requirement |
---|---|
FDA Input Type | Single-ended |
Input AC Supply Voltage | AC Coupled 2-MHz, 2-Vpp Sine Wave |
Component Rating | Space |
FDA Output, ADC Input | 3.2 Vpp |
FDA Output Common Mode | 0.95 V |
Filter | Third-order passive Butterworth low-pass filter with 4-MHz cutoff |
Termination Resistor | No termination resistor |
LMH5485-SEP Radiation Capability | Radiation tolerant up to 30-krad (Si) total ionizing dose (TID) |
Design Description
This space-grade circuit design shows a single-ended-to-differential (SE-to-Diff) ADC driver utilizing the LMH5485-SEP and an analog-to-digital converter (ADC) with a common mode of 0.95 V and an input range of 3.2 Vpp. The LMH5485-SEP is a space-grade, low-power, high-speed fully-differential amplifier that is mainly used to drive high-performance ADCs. High-performance ADCs are low-noise, ultra-low power, high-speed, dual-channel devices that are used in many space applications. Some of these include: imaging, spectroscopy, radar, control loops, instrumentation, and so forth. Since the ADC accepts a differential signal, fully-differential amplifiers (FDA) are a good choice for designing a circuit compared to using two op amps. Aside from providing a balanced output signal, FDAs have other great benefits. Some of these benefits include:
|
|
The following image shows the completed circuit design.
The circuit illustrated in the previous image starts with a single-ended AC source with a 50-Ω source resistance. This source is provided to the LMH5485 fully-operational amplifier. With the feedback resistor values, the gain of the amplifier is 3.2. The output of the FDA then enters a third-order passive Butterworth low-pass filter with a cutoff frequency of 4 MHz before going to the input of the ADC.
Design Steps
Since a termination resistor (Rt) is not used, treat Rt as infinity; therefore, 1/Rt cancels out.
As the equation demonstrates, Rg2 is always twice the resistor value of Rg1.
As seen in design step 4, since a termination resistor (Rt) is not being used, the bottom part of the fraction equals to 1. This equation can be rearranged to solve for Rf. The updated equation follows:
After putting all the components together, 4-MHz 3rd Order Passive Butterworth Low-Pass Filter shows the completed filter. Since this design is differential, the resistors and inductors can be present on both output rails. Therefore, the value of the resistor and inductor is divided by half for each output rail. The input resistors of the filter are 100 Ω. The output resistor named “ADC Load” is a dummy load that represents the internal ADC load which is not part of the filter.
Design Simulations
VIN and VOUT Waveforms
Single-Ended VIN vs Differential VOUT Waveforms shows the input and output of the FDA. Yellow is the input source, red is the positive output, and green is the negative output. The input is 2 Vpp (1 Vpp after the source resistor) and the positive and negative output swing is 1.6 Vpp. Combining the two differential signals, positive and negative, makes the output swing 3.2 Vpp. Note that the output has a common-mode voltage of 0.95 V.
Gain and Phase Bode Plots shows the gain and phase plots of the second-order passive low-pass filter. As the following plot shows, the cutoff frequency is at 4 MHz. This is made to keep the actual cutoff frequency of 2 MHz above –3-dB gain.
Stability
Phase margin of an amplifier is the amount of phase shift when the gain of an amplifier is above 0 dB. An amplifier is considered not stable once the open loop gain falls below 0 dB or when the phase margin drops below 60 degrees. In this case, the open loop gain drops below 0 after 314.84 MHz, with a phase margin of 63.33 degrees as Stability Gain and Phase Bode Plots shows. This is more than enough for the application since the amplifier is only operating at 2 MHz.
Implementing an FDA is a very efficient way to power an ADC. The reduced number of components and increased resistance to external noise and even-order harmonics are some of the great benefits that the FDA offers. The FDA can be intimidating at a first glance, however, when looking into the design steps, the process is very user friendly. In this design, the FDA outputs a desired 3.2 Vpp output with a common mode of 0.95 V. The low-pass filter after the FDA has a cutoff frequency of 4 MHz and since it is a 3rd-order filter, the cutoff is very sharp which removes any unwanted harmonics of the passing frequency.
Additional Resources
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated