SCPA074 September   2024 TPLD1202

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Configuring the Pattern Generator in TPLD Using InterConnect Studio (ICS)
  5. 2Utilizing the Reset Input of the Pattern Generator
  6. 3Generating a Pattern Less Than 16 bits
  7. 4References

Abstract

Whether it is to generate a test pattern or to initialize logic to a known state, the pattern generator (PGEN) macro-cell within TI Programmable Logic Devices (TPLD) can be configured to generate 1-bit to 16-bit patterns. This application note will discuss how to configure and utilize pattern generators within TPLD.