SFFS379A September 2022 – March 2023 TLV766-Q1
This section provides a failure mode analysis (FMA) for the pins of the TLV766-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality. |
B | No device damage, but loss of functionality. |
C | No device damage, but performance degradation. |
D | No device damage, no impact to functionality or performance. |
#GUID-59B67224-3CC4-4810-AE39-411866CAB6F7 shows the TLV766-Q1 adjustable output pin diagram, and #FIG_AML_4HY_KSB shows the TLV766-Q1 fixed output pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TLV766-Q1 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
OUT | 1 | Regulation is not possible. The device operates at current limit and can cycle in and out of thermal shutdown. | B |
NC | 2 | No effect. Normal operation. | D |
FB/SNS | 3 |
(Fixed output.) Regulation is not possible. The device operates at current limit and can cycle in and out of thermal shutdown. (Adjustable output.) The device operates as a switch because the gate of the pass transistor is driven fully on. |
B/B |
GND | 4 | No effect. Normal operation. | D |
EN | 5 | The device is disabled, resulting in no output voltage. | B |
GND | 6 | No effect. Normal operation. | D |
NC | 7 | No effect. Normal operation. | D |
IN | 8 | No power to the device, resulting in no output voltage. | B |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
OUT | 1 | The device output is disconnected from the load. | B |
NC | 2 | No effect. Normal operation. | D |
FB/SNS | 3 |
(Fixed output.) The output voltage is incorrect. (Adjustable output.) The error amplifier input is not connected. The output voltage is indeterminate. |
B/B |
GND | 4 | There is no current loop for the supply voltage. The device is not operational and does not regulate. | B |
EN | 5 | The enable circuit is in an unknown state. The device is either enabled or disabled. | B |
GND | 6 | A very small possibility exists that device turns on even if EN is held low. | B |
NC | 7 | No effect. Normal operation. | D |
IN | 8 | No power is supplied to the device, resulting in no output voltage. | B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|---|
OUT | 1 | NC (pin 2) | No effect. Normal operation. | D |
NC | 2 | FB/SNS (pin 3) | No effect. Normal operation. | D |
FB/SNS | 3 | GND (pin 4) |
(Fixed output.) Regulation is not possible. The device operates at current limit and can cycle in and out of thermal shutdown. (Adjustable output.) The device operates as a switch because the gate of the pass transistor is driven fully on. |
B/B |
EN | 5 | GND (pin 6) | The device is disabled, resulting in no output voltage. | B |
GND | 6 | NC (pin 7) | No effect. Normal operation. | D |
NC | 7 | IN (pin 8) | No effect. Normal operation. | D |
Pin Name | Pin No. | Description of Potential Failure Effects | Failure Effect Class |
---|---|---|---|
OUT | 1 |
(Fixed output.) Regulation is not possible because VOUT = VIN, but no damage occurs because OUT and SNS can handle up to VIN + 0.3 V (max). (Adjustable output.) If FB is tied to OUT, damage is possible on FB. See the Absolute Maximum Ratings table in the product data sheet. If the device is configured with a resistive feedback network, no damage occurs. |
B/A |
NC | 2 | No effect. Normal operation. | D |
FB/SNS | 3 |
(Fixed output.) Regulation is not possible because VOUT = VIN. (Adjustable output.) If VIN is greater than 3 V, the rating for FB (3 V max) is violated and can damage the device. If VIN is less than 3 V and if there is any loading on the device, the output is approximately 0 V. |
A/B |
GND | 4 | No output voltage. System performance depends on upstream current limiting. | B |
EN | 5 | The device is always enabled when the input is powered. | B |
GND | 6 | No output voltage. System performance depends on upstream current limiting. | B |
NC | 7 | No effect. Normal operation. | D |
IN | 8 | No effect. Normal operation. | D |