SFFS618 September   2024 TPS1213-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the TPS1213-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the TPS1213-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TPS1213-Q1 data sheet.

TPS1213-Q1 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The data sheet recommendations for operating conditions, external component selection, and PCB layout are followed.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
EN/UVLO 1 Normal operation. The device is disabled. B
LPM 2 Normal operation. The devices operates in low-power mode. B
INP 3 Normal operation. The G1PD output is low and the external FET is off. B
WAKE 4 WAKE event cannot be reported. B
FLT 5 Overcurrent, UVLO, charge pump UVLO fault diagnostic cannot be reported. B
GND 6 Normal operation. D
CS_SEL 7 Normal operation. D
ISCP/LWU 8 Load wakeup and SCP threshold sets to minimum threshold. B
TMR 9 Overcurrent does not get detected, hence overcurrent protection gets disabled. B
SCP_TEST 10 Normal operation. B
G2 11 With G2 grounded, if the pin voltage between SRC and G exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
BST 12 Gate driver supply does not come up. FETs remain OFF. B
SRC 13 Short to GND protection starts. B
G1PD 14 With G1PD grounded, if the pin voltage between SRC and PD exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
G1PU 15 Gate driver supply gets short circuited. FETs remain OFF. B
CS- 17 Short to GND protection starts. B
CS+ 18 With CS+ grounded, if the pin voltage between CS+ and CS– exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
N.C 19 Normal operation. D
VS 20 Device supply grounded. Device does not power up. B
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
EN/UVLO 1 Internal pulldown brings EN/UVLO to low, disabling the device. B
LPM 2 Internal pulldown brings LPM to low, and the device can operate in low-power mode. B
INP 3 Internal pulldown brings INP to low, pulling G1PD output low. B
WAKE 4 WAKE event cannot be reported. B
FLT 5 Overcurrent, UVLO, charge pump UVLO fault diagnostic cannot be reported. B
GND 6 Device does not power up and is disabled. B
CS_SEL 7 Internal pulldown brings CS_SEL to low, resulting in normal operation. D
ISCP/LWU 8 Load wakeup and SCP threshold sets to maximum threshold. B
TMR 9 Overcurrent response time and auto-retry duration gets reduced to device minimum setting. C
SCP_TEST 10 Internal pulldown brings SCP_TEST to low, resulting in normal operation. B
G2 11 G2 output is not get controlled. B
BST 12 External FET can turn ON and OFF repetitively due to no capacitor connection at the BST pin. B
SRC 13 The external FET is not turned OFF as the FET source is disconnected from the internal pulldown driver. B
G1PD 14 The external FET does not turn OFF, as the FET GATE disconnects from the internal pulldown driver. B
G1PU 15 The external FET does not turn OFF, as the FET GATE disconnects from the internal pulldown driver. B
CS- 17 CS- gets internally clamped to CS+ minus two diode drops. If ISCP/LWU feature is used, the external FET not turning ON is possible due to false overcurrent detection. B
CS+ 18 ISCP/LWU feature does not work. B
N.C 19 Normal operation. D
VS 20 Device does not get powered up and is disabled. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
EN/UVLO 1 2 (LPM) If EN/UVLO is driven high then LPM is detected high making the device function in active mode. B
LPM 2 3 (INP) If LPM is driven high then INP is detected high making the device function in active mode. B
INP 3 4 (WAKE) If device is in active state then FET turns OFF as WAKE is low in active mode B
WAKE 4 5 (FLT) WAKE and FLT are ORed together. B
FLT 5 6 (GND) Fault events are not indicated. B
GND 6 7 (CS_SEL) Normal operation. D
CS_SEL 7 8 (ISCP/LWU) With CS_SEL grounded, load wakeup and SCP threshold sets to minimum threshold. C
ISCP/LWU 8 9 (TMR) TMR and ISCP/LWU thresholds are affected. External FET shuts off at a different threshold than set by ISCP/LWU. During an overcurrent fault the device is in latch-off mode if ISCP/LWU has a < 100kΩ resistor. C
TMR 9 10 (SCP_TEST) SCP_TEST feature gets disabled. B
G2 11 12 (BST) When LPM is driven low, BST (gate driver supply) gets loaded through the internal G2 pulldown switch. Gate driver UVLO hits resulting in turning off the external FETs. B
BST 12 13 (SRC) Gate drive supply gets shorted and external FETs do not turn ON. B
SRC 13 14 (G1PD) Shorting of the pulldown switch (between G1PD and SRC) of the internal gate driver. External FET remains OFF. B
G1PD 14 15 (G1PU) Turn ON and OFF speeds of the external FETs can get impacted. C
CS- 17 18 (CS+) Bypasses the external current sense resistor or FET VDS sensing based on application circuit. SCP features get disabled. B
CS+ 18 19 (N.C) Normal operation. D
N.C 19 20 (VS) Normal operation. D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
EN/UVLO 1 EN/UVLO pin is supply rated. Device remains enabled. B
LPM 2 LPM pin is supply rated. Device operates in active mode depending on supply voltage level. B
INP 3 INP pin is supply rated and is treated driven high. B
WAKE 4 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
FLT 5 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
GND 6 Supply power is bypassed and device does not turn on. B
CS_SEL 7 CS_SEL pin is supply rated. If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. B
ISCP/LWU 8 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
TMR 9 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
SCP_TEST 10 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
G2 11 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
BST 12 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
SRC 13 Output stuck on to supply. B
G1PD 14 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
G1PU 15 If pin voltage exceeds the data sheet range for the pin, the exceedance can cause device damage due to voltage breakdown on the ESD circuit. A
CS- 17 In the application, the external sense resistor or FET VDS sensing gets bypassed. Short circuit protection does not work. A
CS+ 18 No effect. Normal operation. D
N.C 19 No effect. Normal operation. D
VS 20 No effect. Normal operation. D