SFFS700 May 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The LIN module supported is compliant to the LIN 2.1 protocol specification. This module can be programmed to work either as an SCI or as a LIN. The SCI’s hardware features are augmented to achieve LIN functionality. The SCI module is a universal asynchronous receiver-transmitter (UART) that implements the standard non-return to zero format. The SCI can be used to communicate, for example, through an RS-232 port or over a K line.
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):