SLAA334B September 2006 – August 2018 MSP430BT5190 , MSP430F1101 , MSP430F1101A , MSP430F1111A , MSP430F112 , MSP430F1121 , MSP430F1121A , MSP430F1122 , MSP430F1132 , MSP430F122 , MSP430F1222 , MSP430F123 , MSP430F1232 , MSP430F133 , MSP430F135 , MSP430F147 , MSP430F1471 , MSP430F148 , MSP430F1481 , MSP430F149 , MSP430F1491 , MSP430F155 , MSP430F156 , MSP430F157 , MSP430F1610 , MSP430F1611 , MSP430F1612 , MSP430F167 , MSP430F168 , MSP430F169 , MSP430F2001 , MSP430F2002 , MSP430F2003 , MSP430F2011 , MSP430F2012 , MSP430F2013 , MSP430F2013-EP , MSP430F2101 , MSP430F2111 , MSP430F2112 , MSP430F2121 , MSP430F2122 , MSP430F2131 , MSP430F2132 , MSP430F2232 , MSP430F2234 , MSP430F2252 , MSP430F2252-Q1 , MSP430F2254 , MSP430F2272 , MSP430F2272-Q1 , MSP430F2274 , MSP430F233 , MSP430F2330 , MSP430F235 , MSP430F2350 , MSP430F2370 , MSP430F2410 , MSP430F2416 , MSP430F2417 , MSP430F2418 , MSP430F2419 , MSP430F247 , MSP430F2471 , MSP430F248 , MSP430F2481 , MSP430F249 , MSP430F2491 , MSP430F2616 , MSP430F2617 , MSP430F2618 , MSP430F2619 , MSP430F412 , MSP430F413 , MSP430F4132 , MSP430F415 , MSP430F4152 , MSP430F417 , MSP430F423 , MSP430F423A , MSP430F425 , MSP430F4250 , MSP430F425A , MSP430F4260 , MSP430F427 , MSP430F4270 , MSP430F427A , MSP430F435 , MSP430F4351 , MSP430F436 , MSP430F4361 , MSP430F437 , MSP430F4371 , MSP430F438 , MSP430F439 , MSP430F447 , MSP430F448 , MSP430F4481 , MSP430F449 , MSP430F4491 , MSP430F4616 , MSP430F46161 , MSP430F4617 , MSP430F46171 , MSP430F4618 , MSP430F46181 , MSP430F4619 , MSP430F46191 , MSP430F47126 , MSP430F47127 , MSP430F47163 , MSP430F47166 , MSP430F47167 , MSP430F47173 , MSP430F47176 , MSP430F47177 , MSP430F47183 , MSP430F47186 , MSP430F47187 , MSP430F47193 , MSP430F47196 , MSP430F47197 , MSP430F477 , MSP430F478 , MSP430F4783 , MSP430F4784 , MSP430F479 , MSP430F4793 , MSP430F4794 , MSP430F5131 , MSP430F5132 , MSP430F5151 , MSP430F5152 , MSP430F5171 , MSP430F5172 , MSP430F5304 , MSP430F5308 , MSP430F5309 , MSP430F5310 , MSP430F5324 , MSP430F5325 , MSP430F5326 , MSP430F5327 , MSP430F5328 , MSP430F5329 , MSP430F5333 , MSP430F5336 , MSP430F5338 , MSP430F5340 , MSP430F5341 , MSP430F5342 , MSP430F5418 , MSP430F5418A , MSP430F5419 , MSP430F5419A , MSP430F5435 , MSP430F5435A , MSP430F5436 , MSP430F5436A , MSP430F5437 , MSP430F5437A , MSP430F5438 , MSP430F5438A , MSP430F5500 , MSP430F5501 , MSP430F5502 , MSP430F5503 , MSP430F5504 , MSP430F5505 , MSP430F5506 , MSP430F5507 , MSP430F5508 , MSP430F5509 , MSP430F5510 , MSP430F5630 , MSP430F5631 , MSP430F5632 , MSP430F5633 , MSP430F5634 , MSP430F5635 , MSP430F5636 , MSP430F5637 , MSP430F5638 , MSP430F6433 , MSP430F6435 , MSP430F6436 , MSP430F6438 , MSP430F6630 , MSP430F6631 , MSP430F6632 , MSP430F6633 , MSP430F6634 , MSP430F6635 , MSP430F6636 , MSP430F6637 , MSP430F6638 , MSP430FE423 , MSP430FE4232 , MSP430FE423A , MSP430FE4242 , MSP430FE425 , MSP430FE4252 , MSP430FE425A , MSP430FE427 , MSP430FE4272 , MSP430FE427A , MSP430FG4250 , MSP430FG4260 , MSP430FG4270 , MSP430FG437 , MSP430FG438 , MSP430FG439 , MSP430FG4616 , MSP430FG4617 , MSP430FG4618 , MSP430FG4619 , MSP430FG477 , MSP430FG478 , MSP430FG479 , MSP430FW423 , MSP430FW425 , MSP430FW427 , MSP430G2001 , MSP430G2101 , MSP430G2102 , MSP430G2111 , MSP430G2112 , MSP430G2121 , MSP430G2131 , MSP430G2132 , MSP430G2152 , MSP430G2201 , MSP430G2201-Q1 , MSP430G2211 , MSP430G2212 , MSP430G2221 , MSP430G2231 , MSP430G2231-Q1 , MSP430G2232 , MSP430G2252 , MSP430G2302 , MSP430G2312 , MSP430G2332 , MSP430G2352 , MSP430G2402 , MSP430G2432 , MSP430G2452 , MSP430L092
Flash memory is a widely used, reliable, and flexible nonvolatile memory to store software code and data in a microcontroller. Failing to handle the flash according to data-sheet specifications can result in unreliable operation of the application. This application report explains the physics behind these specifications and also gives recommendations for the correct management of flash memory on MSP430™ microcontrollers (MCUs). All examples are based on the flash memory used in the MSP430F1xx, MSP430F2xx, and MSP430F4xx microcontroller families.
MSP430 is a trademark of Texas Instruments.
All other trademarks are the property of their respective owners.
Flash memory is one of the most popular nonvolatile memories to store program code and constant data values. Many microcontrollers, such as the MSP430 family of microcontrollers, have integrated flash memory for nonvolatile data storage. But there are big differences in behavior and performance of flash memory cells. This report explains the parameters and behavior of the ultra-low-power flash memory used in the MSP430F1xx, MSP430F2xx, and MSP430F4xx families.
A flash memory cell is based on a transistor with a floating gate. Figure 1 shows a simplified schematic of a flash memory cell. The ultra-low-power flash memory cell of a MSP430 is slightly modified, but the basic function is the same.
Underneath the control gate is an additional floating gate. This floating gate is either fully charged or discharged. Charging and discharging this floating gate is done with high energy through the oxide. The amount of charge in the floating gate influences the threshold of the transistor, which generates a logical 1 or 0 when this flash cell is read.
Erasing a flash cell, as shown in Figure 2, is positive charging the floating gate. A positive-charged floating gate results in reading a logical 1 from this erased memory cell. Negatively charging the floating cell, as shown in Figure 3, means programming this cell. The CPU reads from a programmed cell the logical value 0. For erasing and programming, high energy is needed to transport the charge through the oxide by FN tunneling for erasure or channel hot electron (CHE) injection for programming.
The smallest unit that can be erased in a flash memory is a complete flash segment. Erasing flash means generating logical 1s in the memory. The MSP430 main flash memory has a segment size of 512 bytes. All MSP430 devices also have some smaller 64-byte or 128-byte flash segments. This area of the flash is called the information memory. In most applications, the main memory stores program code and constant data values, and the information memory is used for calibration data, serial numbers, etc. Except for the segment size, there is no difference between the main and the information memory. Hence, both can store program code or constant data values or both.
Programming flash memory generates logical 0 values in the flash memory cell. Programming can be performed bit, byte, or word wise. Flash segment size has no influence on programming of flash cells.
Only logical 0 can be written as single bits, bytes, or words. Because writing logical 1 in flash memory is only possible with erasing the memory, 1s can only be written segment-wise.
A high voltage is needed to program and erase flash memory. All MSP430 devices have an integrated charge pump and automatically generate this high voltage, when necessary. Also, a flash timing generator for automatic generation of erase and programming sequences is integrated in every MSP430. Hence, MSP430 flash programming is done without any external components. For programming and erasure, it only is important to keep the supply voltage VCC within the data sheet limits and to program the input clock frequency of the flash timing generator according to data sheet requirements.