SLAA936A September 2020 – March 2021 TAS2563
Located under the Audio Processing page, the biquad stage comprises ten biquad filters which feature an array of filter options such as first-order or second-order low-pass and high-pass, notch, bass and treble shelf, and band pass. The configuration options vary by filter type. The most typical filter is the equalizer, where the range can be set as the bandwidth or Q.
Figure 2-15 shows an example setting for a bandpass filter using the EQ control.