SLAA937 June 2020 TAS2110 , TAS2562 , TAS2563 , TAS2564
Some audio applications, like automotive or industrial, require devices to operate in harsh environments where temperature is higher than consumer electronic goods typically endure. Most of the modern devices have protection schemes; however this typically stops the device from functioning or disables it completely. Once the temperature is back in a safe region, the device needs to be reinitialized.
Thermal Foldback feature on TAS2110, TAS2562, TAS2563 and TAS2564 has the advantage of allowing the device to keep operating and playing audio in increasing temperature situations. The device monitors the die temperature and automatically limits the audio signal above a set threshold. This will ultimately allow the device to keep or reduce its temperature while it is still operating. This is specially useful in fire & security applications as well as automotive applications where ambient temperature can be considerably higher than other applications but the system has to be fully operational. In any case, the over-temperature protection will shut down the device if the die temperature continually increases in order to prevent damages. In addition, over-temperature protection is an auto-retry feature so the device does not have to be reinitialized when temperature is back to a safe region.