SLAAEC6A October 2023 – January 2024
The TAx5x1x-Q1 EVM GUI is an application that installs into the PPC3 framework. PPC3 must be installed before downloading the TAx5x1x-Q1 EVM GUI. Click here to download the PPC3 and request access. If the PPC3 is already installed, proceed to TAx5x1x-Q1 EVM GUI. Figure 4-1 shows the setup directory for the PPC3 installation.
Open the PPC3 installer and follow the instructions in the setup wizard.