SLAU835A December   2020  – February 2022 TAS2563

 

  1. Trademarks
  2. Description
  3. Specifications
  4. Software
  5. Device Configuration
    1. 5.1 Default Jumper Settings
    2. 5.2 Mono Setup
  6. Digital Audio Interfaces
  7. Multi-Channel Configuration
  8. EVM Schematics
  9. EVM Layer Plots
  10. 10Bill of Materials
  11. 11Revision History

Mono Setup

Use the following instructions to complete a mono setup:

  1. Install PPC3 with the TAS2563 plug-in.
  2. Connect a speaker to J11.
  3. Connect a 5 V supply to connector J16 or J31.
  4. Connect a Micro USB Cable from PC to TAS2x63EVM.
  5. Verify that TI USB Audio UAC2.0 is the default playback device by opening the sound dialog from the Windows Control Panel.
    GUID-E48F20EF-13A4-45BD-B014-CD1189E5D543-low.png Figure 5-2 Windows Playback Devices
  6. Set the maximum bit depth using the Texas Instruments USB Audio Device Control Panel found in the system tray.
    GUID-3E9FF61C-135B-4A60-8C30-95B3018C3E76-low.png Figure 5-3 Texas Instruments USB Audio Device Control Panel
  7. Set the sampling rate.
    • Right click TI USB Audio UAC2.0
    • Select Properties
    • Click advanced tab
    • Select Rate
      GUID-B35C8966-EC33-4D2A-81B3-ABB40A8074B7-low.png Figure 5-4 Windows Playback device Sample Rate
  8. Configure the device using the TAS2563 PPC3 Plug-in.