SLAU846A June 2023 – October 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1
In SHUTDOWN mode, the entire regulated core supply of the device is disabled and the device wakes only from a wake-capable IO that is configured for wakeup, from NRST, or from a debug connection. The IO wake mechanism for exiting SHUTDOWN is managed by IOMUX and is level based. The 5-V tolerant open-drain IOs, high-drive IOs, and certain standard-drive IOs include the additional wakeup logic that can be used to wake the device from a SHUTDOWN operating mode upon a level match.
To configure a wake-capable IO for wakeup from SHUTDOWN mode:
After the previous configuration, SHUTDOWN mode can be entered through the appropriate command in SYSCTL. Pins on the device that contain digital IO controlled by IOMUX retain their current state when the device enters into SHUTDOWN. While the digital IO state is latched upon entry into SHUTDOWN mode, the IOMUX configuration registers (all PINCMx registers) lose their contents as the regulated core supply is shut down.
After SHUTDOWN is entered, a level match on any pin configured for wakeup triggers the exit sequence from SHUTDOWN. When the device exits SHUTDOWN, a BOR-level reset occurs but the state of the digital IO remains latched through the reset, keeping the IO state that was present upon entry into SHUTDOWN. This state is held until the IO are released in SYSCTL. After the BOR, SYSCTL captures the cause of the reset as a SHUTDOWN exit so that software can identify this and take appropriate action to reconfigure the device.
If multiple pins were configured for wakeup from SHUTDOWN, application software can determine which wakeup-configured IO generated the wake by polling the WAKESTATE bit in any IOs that were enabled for wake before the SHUTDOWN exit.
Application software must apply the following process to restore the IO state upon exit from SHUTDOWN: