SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
To optimize the number of pins used by the LCD, it is possible to connect more than one segment to the same segment pin. To do this, the common pins of the segments sharing the same segment pin have to be connected to different common pins. This feature is referred to as different mux option. If the segment pins are not shared between multiple segments, then such configuration is called as a static configuration Figures below show examples of Static, Mux 2, Mux 3 and Mux 4 configurations
The above diagrams on mux configurations illustrates the segment pins being connected to more than one com line in figures b,c and d. Thereby, depending on the muxing option, the number of COM pins is determined; for example 1 COM pin for static configuration, 2 COM pins for 2-Mux configuration and so on). As the muxing modes increase, the number of pins used to drive a given number of segments reduce. In case of non static configuration, the waveform applied on SEG and COM lines is time division multiplexed.