SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
In static mode, VA, VB, VC and VD either take the value of V1 or V5 (2 levels). Figure below depicts one frame of LCD. Signals VA and VB determine the segment waveform, VC and VD determine the waveform on the common line. To generate these waveforms, 2 switch control waveforms are generated as shown in the diagram below. From these 2 waveforms, nonoverlapping switch control signals (*_PHASE1 and *_PHASE2) are generated.
As can be seen from the timing diagram, in static mode three switch control signals VA-SW_CTRL, VB-SW-CTRL and VD-SW-CTRL signals are used. VB and VD switch control are complimentary to VA switch control.
As can be seen from the timing diagram above, in static mode three switch control signals VA-SW_CTRL, VB-SW-CTRL and VD-SW-CTRL signals are used. VB and VD switch control are complimentary to VA switch control. Following table summarizes how the various switches in the switch matrix are controlled using these signals in static mode
Switch | Switch Control
(Switch is closed when switch control is high) |
Description |
---|---|---|
VA-V1 | VA-SW-CTRL-PHASE2 | Vlcd on VA |
VA-V5 | VA-SW-CTRL-PHASE1 | V5 on VA |
VB-V2 | Switch open in static mode | |
VB-V3 | Switch open in static mode | |
VB-V4 | Switch open in static mode | |
VB-VD | Always closed in static mode | VB and VD waveforms are the same. |
VC-V4 | Switch open in static mode | |
VC-V2 | Switch open in static mode | |
VD-V1 | VD-SW-CTRL-PHASE2 | Vlcd on VD |
VD-V5 | VD-SW-CTRL-PHASE1 | V5 on VD |
VA-VSS | Switch closed, when LCDON is 0. | |
VB-VSS | Switch closed, when LCDON is 0. | |
VC-VSS | Switch closed, when LCDON is 0. | |
VD-VSS | Switch closed, when LCDON is 0. |