SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
The AESADV module provides a trigger source which can be configured to source DMA trigger 0. The DMA0 trigger events from the AES are given in Table 28-506. When the DMA0 channel is needed by the AES for block cipher operations, the DMA0 trigger should be unmasked in the IMASK register of DMA_TRIG_DATAIN and the DMA should be configured as needed to support the AES operation.
Index (IIDX) | Name | Description |
---|---|---|
0 | NO_INTR | No DMA Trig0 event pending |
1 | TRIG0 | DMA Trigger for Data Input |
The DMA trigger 0 event configuration is managed with the DMA_TRIG_DATAIN event management registers. See Section 7.2.5 for guidance on configuring the event registers for DMA triggers.