SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
Two periodic alarms are provided, and can be configured to generate two periodic time bases for the application.
The RT0PS periodic alarm can be configured to generate a periodic interrupt at one of the following rates: 4096Hz, 2048Hz, 1024Hz, 512Hz, 256Hz, or 128Hz. The RT0PS period is set by the RT0IP bits in the PSCTL register. The RT0PS event sources the RT0PS interrupt.
The RT1PS periodic alarm can be configured to generate a periodic interrupt at one of the following rates: 64Hz, 32Hz, 16Hz, 8Hz, 4Hz, 2Hz, 1Hz, or 0.5Hz. The RT1PS period is set by the RT1IP bits in the PSCTL register. The RT1PS event sources the RT1PS interrupt.