SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
The following steps are used to configure the main timer cross trigger (which is TIMGx in this example):
Configure the main timer (which triggers other secondary timers) for the desired function, such as PWM output generation or using compare mode, to trigger other peripherals. See Section 23.2.5 for how to configure for PWM generation.
Figure 23-39 shows the connection logic and registers.