SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
Peripheral interrupt functionality is managed by several components on the device:
MSPM0 devices include an Arm nested vectored interrupt controller (NVIC) with the Cortex-M0+ CPU for managing peripheral interrupts. The NVIC operation is tightly integrated with the processor and supports up to 32 native peripheral interrupt sources.
In addition to the NVIC, interrupt grouping modules can be present on a device to enable interfacing of more than 32 peripheral interrupts to the NVIC. High-priority interrupt sources that might require preemption capability are mapped directly to the NVIC and behave like normal NVIC interrupts. Lower priority interrupt sources which do not commonly require preemption capability are mapped to an interrupt grouping module, the output of which is then mapped to the NVIC as a native NVIC interrupt source. This routing arrangement is shown in Figure 3-3.
The wake-up controller (WUC) determines if the PD1 power domain (containing the processor) needs to be powered up to service a peripheral interrupt if the PD1 domain is powered down in STOP or STANDBY mode.