SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
Peripherals in power domain 1 (PD1) will be forced to a disabled state by SYSCTL upon entry into a STOP or STANDBY low-power mode. As such, these peripherals will not be available for use in STOP or STANDBY.
Most PD1 peripherals will retain their configuration settings after being automatically disabled, such that re-configuration is not required upon exit from STOP or STANDBY mode. See the peripheral-specific chapter in this guide for details on which peripheral registers are retained through STOP and STANDBY mode for PD1 peripherals.
If a PD1 peripheral was multiplexed to an IO pin (through the IOMUX) in an output configuration, the last valid output state (logic 0 or logic 1) from the peripheral to the IO is latched upon entry to STOP or STANDBY mode. This prevents external circuits from being disturbed by SYSCTL disabling a peripheral during low-power operation. Upon exit from STOP or STANDBY mode, the IO is again connected to the peripheral as the peripheral becomes re-enabled.