SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
When shadow compare is enabled for updating the capture/compare register (TIMx.CC), the value written to the respective compare register is first stored into a shadow compare register and then transferred to the compare register at different events configured by setting the TIMx.CCCTL_xy[0/1].CCUPD bits.
Additionally, the capture/compare action register (TIMx.CCACT) has the ability to update the action at different events configured by setting the TIMx.CCCTL_xy[0/1].CCACTUPD bits.
Table 23-16 shows the settings for configuring when shadow compare and actions occur at different events.
Bit Field | Value | Description/Comment |
---|---|---|
CCUPD / CCACTUPD | 0 | The value written to TIMx.CC register take effect immediately. |
1 | The value written to the TIMx.CC register is stored in a shadow compare register and gets transferred to the TIMx.CC register in the TIMCLK cycle following a zero event (TIMx.CTR value equals 0). | |
2 | The value written to the TIMx.CC register is stored in a shadow compare register and gets transferred to the TIMx.CC register in the TIMCLK cycle following a compare (down) event (TIMx.CTR value equals TIMx.CC) | |
3 | The value written to the TIMx.CC register is stored in a shadow compare register and gets transferred to the TIMx.CC register in the TIMCLK cycle following a compare (up) event (TIMx.CTR value equals TIMx.CC) | |
4 | The value written to the TIMx.CC register is stored in a shadow compare register and gets transferred to the TIMx.CC register in the TIMCLK cycle following a zero or load event (TIMx.CTR value equals 0 or TIMx.CTR equals TIMx.LOAD). Note: this update mechanism is defined for use only in up/down counting mode. | |
5 | The value written to the TIMx.CC register is stored in a shadow compare register and gets transferred to the TIMx.CC register in the TIMCLK cycle following a zero event and the repeat count equaling zero (TIMx.CTR value equals 0 and TIMx.RC equals 0) | |
6 | The value written to the TIMx.CC register is stored in a shadow compare register, and gets transferred to the TIMx.CC register in the TIMCLK cycle following a trigger pulse. See Section 23.2.7. |
Figure 23-25 shows an example of how shadow load and shadow compare takes effect at the zero event for both the TIMx.LOAD and TIMx.CC value in up/down counting mode.