SLAU874 October 2022 TPA3223
The TPA3223EVM supports both AD modulation as well as HEAD modulation. In AD mode, each of the two half-bridge outputs are continuously switching. AD mode is the default mode for the TPA3223EVM. The EVM also supports HEAD mode modulation. HEAD mode also switches both half bridge outputs but also optimizes the switching for lower power loss at idle as well as increased EMI performance at cost of some performance. The device accomplishes this by reducing its duty cycle at idle and while playing small signals. At higher output levels HEAD mode will also reduce the switching on one of the half bridges. The modulation mode can be controlled through jumper J6 on the EVM as follows:
J6 Jumper State | Modulation Mode |
---|---|
IN | AD Mode |
OUT | HEAD Mode |
More information on the differences between HEAD mode and AD mode as well as performance data is found in the TPA3223 data sheet (SLASEF0).