SLAU943 July 2024 AMC6V704
Figure 4-5 shows the Low Level Configuration page of the AMC6V704EVM-GUI. This page allows access to low-level communication directly with the respective AMC6V704 device registers.
The Register Map section in the center of the window lists all the registers, grouped by the pages in the device. The GUI automatically addresses the correct page based on the register selected. Selecting a register on the Register Name list shows a description of the values in that register, as well as information on the register address, default value, size, and current value. Data are written to the registers by entering a value in the value column of the GUI.
To store the values of the register map locally, select Save Configuration under the File menu option. The stored configuration files can be recalled and loaded by selecting Open Configuration.
Figure 4-6 shows the four configuration buttons provided on the Low Level Configuration page that allow the user to read from and write to the device registers:
The Write Modified button is enabled only in Deferred Update Mode. Deferred Update Mode initiates a write operation only when the Write Selected or Write Modified buttons are pressed. By default, Immediate Update Mode is selected for the Low Level Configuration page write operations.
The AMC6V704 SDO pin must be enabled in the SDO_EN register before reading any device registers.