SLLU335A August 2021 – January 2022 MCF8316A
MCF8316A provides four options to configure the input speed command.
PWM input on SPEED pin by varying duty cycle of input signal
Frequency input on SPEED pin by varying frequency of input signal
Analog input on SPEED pin by varying amplitude of input signal
Over I2C by configuring SPEED_CTRL
Configure the speed input [SPEED_MODE] register to select the appropriate speed input mode.
If PWM input on SPEED pin is chosen as the speed input, configure SPEED_RANGE_SEL to select the PWM frequency range.
If Frequency input on SPEED pin is chosen as the speed input, configure INPUT_MAXIMUM_FREQ to select the maximum PWM frequency. For example, if 10 kHz is chosen as maximum PWM frequency, 10 kHz PWM signal on SPEED pin will correspond to 100% speed command.
To command the speed via I2C, toggle the “Enable Speed Control via I2C” in the I2C Control Section in GUI.