SLLU350 April 2022 TUSB1142
The EVM board can be powered from either the Micro-B receptacle (J1) VBUS or from an external power supply through the barrel jack (J2). The EVM defaults to being powered from the Micro-B receptacle VBUS.
If powering EVM from barrel jack, make sure R54 is unpopulated. Once removed, a jumper will need to be placed across JMP19 pins 1 and 2.
The USB Type-C receptacle VBUS uses TPS25820 as the VBUS power switch needed for USB Type-C systems. Power is sourced from the Micro-B receptacle VBUS by default. JMP1 can be used to change the power source at the USB Type-C receptacle VBUS pins.
If powering USB Type-C VBUS from barrel jack or other source, make sure R14 is unpopulated. Once removed, a jumper will need to be placed across JMP1 pins 1 and 2 to use power form the barrel jack. If a different external power source is used, connect the source directly to JMP 1 pin 2.