All parameters are measured according to the conditions described in theSpecifications section.
1. Input resistor RI = 150kΩ gives a gain of 6 dB which is used for all the graphs
2. CI was shorted for any common-mode input voltage measurement. All other measurements were taken with CI = 0.1-μF (unless otherwise noted).
3. CS1 = 0.1μF is placed very close to the device. The optional CS2 = 10μF is used for datasheet graphs.
4. The 30-kHz low-pass filter is required even if the analyzer has an internal low-pass filter. An RC low-pass filter (1kΩ, 4700pF) is used on each output for the data sheet graphs.
Figure 28. Test Setup for Typical Application Graphs