A resistor pair is made up of two resistors connected in series making up a resistor divider. With matched pairs, each pair functions independently and is made up of an RIN and an RG with RIN1 = RIN2 and RG1 = RG2. A tap point can be found between the resistors of each divider, labeled RMID1 and RMID2 in the Functional Block Diagram. Additionally, one of the two GND pins can be used to bias the substrate for best AC performance.
To determine the value of the resistors, consider the ratio of the RES11Axx device in question. The divider ratio for a resistor pair is RIN divided by RG, where RIN is fixed to 1kΩ for all RES11A-Q1 and RG is the variable gain resistor that sets the dividing ratio. Each orderable part number (OPN) is associated with a different ratio, as noted in the Table 1 table. For example, a RES11A20 has a 1:2 ratio, thus the resistor has a 1kΩ RIN and a 2kΩ RG. For additional specifications see the RES11A-Q1 Automotive, Matched, Thin-Film Resistor Dividers With 1-kΩ Inputs data sheet.
OPN | RIN (Nominal) | RG (Nominal) | Maximum Differential Divider Voltage (RINX Pin to RGX Pin)(1) |
---|---|---|---|
RES11A00 | 1kΩ | 10kΩ | 44.7V |
RES11A10 | 1kΩ | 1kΩ | 24.4V |
RES11A15 | 1kΩ | 1.5kΩ | 20.3V |
RES11A16 | 1kΩ | 1.667kΩ | 19.9V |
RES11A20 | 1kΩ | 2kΩ | 18.3V |
RES11A25 | 1kΩ | 2.5kΩ | 28.4V |
RES11A30 | 1kΩ | 3kΩ | 32.5V |
RES11A40 | 1kΩ | 4kΩ | 30.5V |
RES11A50 | 1kΩ | 5kΩ | 29.9V |
RES11A90 | 1kΩ | 9kΩ | 40.7V |
The RES11A-Q1 features a ±0.05% maximum ratio tolerance (tD1 and tD2) meaning that the ratio of RIN1:RG1 and RIN2:RG2 are at most 0.05% off of the specified ratio values at a room temperature of 25°C. The initial tolerance (tabs) of 14% refers to the part-to-part variation of the individual resistors to the nominal or printed resistance. The four resistors within the device track each other much more closely, with a typical absolute error span of 235 ppm. This means a RES11A-Q1 (which has a nominal RIN1 of 1kΩ) can have an RIN1 value as high as 1140Ω; however, because of the maximum ratio tolerance specification this means all other resistors (RIN2, RG1, RG2) have values approximately 14% above the nominal values of these resistors.
Consider a standard differential amplifier as Figure 3 shows. When simplified to R1 = R2, and R3 = R4, CMRR can be expressed as CMRR(dB) = 20×log[(1+R3 / R1) / (4T / 100)] where T is resistor tolerance in percent. This means CMRR is expected to be only 54dB in a unity gain configuration (R1 = R3) with unmatched 0.1% tolerance resistors. If both divider ratios are matched to a 0.05% ratio tolerance then the value for T in this formula is 0.025% resulting in an improved CMRR of 66dB. See the application information section in the RES11A-Q1 data sheet to learn more about how this number is calculated. An operational amplifier has infinite CMRR, which is a specification pertaining to the amount of the common mode signal present at the output of an amplifier. Ultimately, CMRR is a factor impacting the output signal noise. Learn more about CMRR with the Common-mode rejection ratio TI Precision Labs video on this topic.
Difference Amplifier
Utilizing an operational amplifier such as the OPA392 and a single RES11A-Q1 in the Difference Amplifier Configuration yields a differential amplifier topology including differential inputs and a single-ended output. The gain of the amplifier can be calculated by the formula in Equation 1.
Instrumentation Amplifier
Utilizing two operational amplifiers such as OPA392 and a single RES11A-Q1 in the Instrumentation Amplifier Configuration yields an instrumentation amplifier topology with two high-impedance inputs and differential output. In some cases, a weak path for input bias current is needed(1). The gain of the amplifier is calculated using Equation 2.
Utilizing two operational amplifiers such as OPA392 and a single RES11A-Q1 as illustrated in Figure 6 yields an instrumentation amplifier topology with two high-impedance differential inputs, one single-ended output, and a reference input. is important to simulate the design to check that the input common mode ranges and output swings meet the requirements of the desired application. The gain of the amplifier is calculated with Equation 3.
Fully-Differential Amplifier
A fully-differential amplifier requires resistors to set the gain as Figure 7 illustrates. The ratio between these resistors determines the gain, thus matching is important to make sure the circuit behaves as intended. Equation 4 shows the formula for gain in this configuration.
The maximum sustained differential voltage rating per divider is determined by a number of factors, including the maximum junction temperature and the self-heating associated with a given voltage and divider impedance. See the specifications section of the RES11A-Q1 Automotive, Matched, Thin-Film Resistor Dividers With 1-kΩ Inputs data sheet for more details.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated