To debug connection issues to BQStudio, first
verify that you are running the newest version of BQStudio, which
is the BQSTUDIO-TEST file.
Then proceed to follow the steps from the Quick Start Section of the EVM
- Connect a power supply between BAT+ and
BAT-.
- Connect your computer via a USB cable to the EVM.
Three green LEDs are turn on when the computer is connected.
- Check BQStudio’s Dashboard to verify that the
on-board microntroller is connected and which firmware is using.
- Only have one EVM connected to your laptop for
each unique window of BQStudio being used.