SLUAAQ5 May 2024 BQ769142 , BQ76942 , BQ76952 , BQ76972
Is recommended that the input resistors be between 20 and 100Ohms. This is to limit the total current flowing during balancing to protect the device from overheating while still balancing at a reasonable speed. Due to the higher current that flows through VC16, is recommended this to be kept at 20 ohms regardless of the other pins resistances. In addition, is also recommended to add a 0.22uF capacitor at each cell input.