In most situations, the microcontroller can set the desired parameters after power-up for typical operations without needed OTP programming. However, if a different default value is needed on power-up, the device has an OTP memory that the customer's production line can change these default values. There are three common use cases:
- Configuring REG1/2 LDOs during Startup: This is
most often used when REG1 needs to power the microcontroller of the system. The
BQ7695202 have REG1 defaulting to 3.3V without the user having to modify the OTP
memory.
- Changing Communication Modes: If the user decides
to change communication modes, this can be adjusted in the OTP memory. The table
in Section 1 highlights the different preconfigurations that are available for
the BQ769x2 family.
- Using the BQ769x2 in Stand-Alone Mode: If the
device is not being used in conjunction with a microcontroller, all
modifications must be made in the OTP memory to not be wiped when the device
enters SHUTDOWN mode. Therefore OTP programming allows permanent modifications
to allow the device to operate alone.