SLUAAT3 November 2023 TPS56837
Both TPS56837 and TPS56637 are 10-pin, VQFN-HR, RPA packages. Figure 4-1 are the pinouts of TPS56837 and TPS56637. The only difference between the two is pin 5.
The pin 5 of TPS56837 is a SS pin, which is the soft-start time configuration pin. Leaving SS pin floating leads to default 1.8-ms soft start time. Connecting an external capacitor between SS and AGND leads to longer soft start time.
The pin 5 of TPS56637 is a NC pin. NC pin must not be connected and stay floating during use.