SLUSDD4B April 2019 – December 2020
PRODUCTION DATA
The voltage stress by the converter on the diode can be found with Equation 20.
Note that any diode picked should have a voltage rating of well above this value as it does not include parasitic spikes in the equation. The UC1843B-SP diode was picked to have a voltage rating of 60 V.