SLUU224A May 2005 – March 2022 TPS40100
Fan
This evaluation module includes components that can get hot to the touch. A small fan capable of 200–400 LFM is required to reduce component surface temperatures to prevent user injury. The EVM should not be left unattended while powered or probed while the fan is not running.
Oscilloscope
A 60-MHz or faster oscilloscope can be used to monitor many points on the EVM. For output ripple voltage measurements, the Oscilloscope should be set for the following to take output ripple measurements:
Function Generator
A function generator capable of sourcing a 0-V to 5-V square wave at frequencies past 400 Khz.