Adjust the input supply to provide 4 VDC, current limited to 1 ADC.
Apply the input voltage to the EVM. See Figure 5-1 for overview of the EVM and its connections.
Launch the Fusion GUI software. See the screen
shots in Section 9 for more information.
Configure the EVM operating parameters as desired.
VSET pin is pulled up to BP3 on the EVM, so the VOUT_COMMAND at boot up is restored from the internal EEPROM. The SYNC/RESET_B pin is configured to SYNC function under this setup. In order to use VSET or RESET_B function, proper resistor of R19 should be populated and resistor R18 should be removed. Please see Datasheet for more details.
S1 on the EVM provides the option to use the external temperature sensor Q1 on the EVM.
Note:
To read the external temprature value on PMBus, the bit 8 (SS_DET_DIS) in (E5h) MFR_SPECIFIC _21 register needs to be set to 1. Otherwise, the READ_TEMPERATURE_2 will always return 25°C.
With an input of 4 VDC, the internal configuration circuitry will be powered and active but the device will still be in UVLO and outputs off.