SLUUC48A February 2020 – February 2022 TPS546B24A
Figure 10-2 shows the General Settings that can be used to configure the following:
After clicking Write to Hardware to make changes to one or more configurable parameters, the changes can be committed to nonvolatile memory by clicking Store Config to NVM. This action prompts a pop-up, and if confirmed, the changes are committed to nonvolatile memory to store all the modifications in non-volatile memory.
Both the loop controller device and the loop follower device are tied to same bus interface. In a two-phase stacking system, the controller device will receive and respond to all PMBus communication and follower devices do not need to be connected to the PMBus. If the controller receives commands that require updates to the PMBus registers of the follower, the controller will relay these commands to the followers. All commands on this tab are for PHASE = 0xFF.