SLUUC74 May   2021 BQ25720 , BQ25723

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 EVM Features
    2. 1.2 General Description
  3. 2Test Summary
    1. 2.1 Definitions
    2. 2.2 Equipment
    3. 2.3 Equipment Setup
    4. 2.4 Procedure
      1. 2.4.1 Charge Function
      2. 2.4.2 OTG Function
  4. 3Bill of Materials, Board Layout, and Schematics
    1. 3.1 Bill of Materials
    2. 3.2 Board Assembly Layout
    3. 3.3 Schematic

Definitions

This procedure details how to configure the BMS035 evaluation board. For the test procedure, the following naming conventions are followed. Refer to the BMS035 schematic for details.

VXXX: External voltage supply name (VADP, VBT, VSBT)
LOADW: External load name (LOADR, LOADI)
V(TPyyy): Voltage at internal test point TPyyy. For example, V(TP12) means the voltage at TP12.
V(Jxx): Voltage at jack terminal Jxx.
V(TP(XXX)): Voltage at test point “XXX”. For example, V(ACDET) means the voltage at the test point which is marked as “ACDET”.
V(XXX, YYY): Voltage across point XXX and YYY.
I(JXX(YYY)): Current going out from the YYY terminal of jack XX.
Jxx(BBB): Terminal or pin BBB of jack xx
Jxx ON : Internal jumper Jxx terminals are shorted
Jxx OFF: Internal jumper Jxx terminals are open
Jxx (-YY-) ON: Internal jumper Jxx adjacent terminals marked as “YY” are shorted
Measure: → A,B Check specified parameters A, B. If measured values are not within specified limits, the unit under test has failed.
Observe → A,B Observe if A, B occurs. If they do not occur, the unit under test has failed.

Assembly drawings have locations for jumpers, test points, and individual components.