The EVM includes two charge pump
options to enable powering the TPS546B24A from a single 3.3-V input supply. The
operation of these charge pumps is discussed in the Powering the TPS546D24A Device Family from a Single 3.3-V Input Power
Supply Application Report.
Before implementing the following instructions
to use one of the charge pump circuits, it is first necessary to modify the
conditions that enable power conversion. By default, the EVM is configured to start
switching when PVIN goes above 4.7 V based on the R1 and R2 voltage divider to the
EN pin. Increasing R2 from 8.66 kΩ to 16.2 kΩ sets the enable threshold to
approximately 3.0 V. An alternative method is to use the Fusion GUI to change the
On/Off Config setting to Always Converting such that the device is
enabled whenever power is present, regardless of the state of the EN pin or the
OPERATION command. The configuration screen is shown in Figure 10-3. Be sure to Store Config to NVM after writing the change
to hardware such that the setting persists after power is removed and reapplied.
To use the discrete charge pump, modify the EVM as follows:
- Modify the enable threshold or
On/Off Config of the device as described previously.
- Set SYNC pin as an output. This can be accomplished by doing either of
the following:
- Populate ADRSEL pin-strap resistor divider with R9 = 2.05 kΩ and R10 =
10 kΩ.
- Use Fusion GUI to set the
SYNC_DIR bits of the SYNC_CONFIG register to 01b:
Enable SYNC OUT. This register can be set from the All
Config tab in Fusion GUI, shown in Figure 10-8. Be sure to Store Config to NVM after writing
the change to hardware.
- Remove the jumper JP3 to disconnect AVIN from both the external AVIN header (T1)
and from PVIN.
- Populate the resistors R26, R27, and R29 with 0-Ω resistors.
- Apply PVIN input voltage. Note that the output voltage of the discrete charge
pump will be approximately 2 × PVIN (minus two diode drops). Pay careful
attention that the applied PVIN remains below 9 V such that the generated AVIN
does not exceed the 18-V rating of the converter IC.
To use the charge pump IC TPS60150, modify the EVM as follows:
- Modify the enable threshold or
On/Off Config of the device as described previously.
- Remove the jumper JP3 to disconnect AVIN from both the external AVIN header (T1)
and from PVIN.
- Populate the resistors R30 and R31 with 0-Ω resistors.
- Apply PVIN input voltage. Pay careful attention that the applied PVIN remains
below the 5.5-V input rating of the TPS60150 charge pump IC.
Note: Only one charge pump circuit should be connected and used at a time. Remove the
0-Ω resistors that connect the charge pump to PVIN and AVIN (and SYNC for the
discrete charge pump) before connecting the other charge pump, or before testing
other conditions with higher input voltages that do not require the charge
pump.