All trademarks are the property of their respective owners.
The Texas Instruments LMR51420EVM evaluation module (EVM) helps designers evaluate the operation and performance of the LMR51420 wide-input buck regulator.
The Texas Instruments LMR51420EVM evaluation module (EVM) helps designers evaluate the operation and performance of the LMR51420 wide-input buck regulator.
The EVM contains one DC/DC converter (see Table 1-1).
CONVERTER | EVM | DEVICE | PACKAGE |
---|---|---|---|
U1 | LMR51420EVM | PLMR51420 | SOT23-6 |
This section describes the jumpers and connectors on the EVM and how to properly connect, set up, and use the LMR51420EVM.
If other outputs need to be configured, leave jumper J1 unconnected and adjust the feedback resistors using the Equation 1.
where