This user's guide provides detailed testing instructions for the BQ25620 and BQ25622 evaluation modules (EVM). Also included are descriptions of the necessary equipment, equipment setup, and procedures. The reference documentation contains the printed-circuit board layouts, schematics, and the bill of materials (BOM).
Throughout this user's guide, the abbreviations EVM, BQ25620EVM, BQ25622EVM, BMS050, and the term evaluation module are synonymous with the BMS050 evaluation module, unless otherwise noted.
All trademarks are the property of their respective owners.
The BMS050 evaluation module (EVM) is a complete charger module for evaluating the BQ25620 and BQ25622 devices. The BQ25620 and BQ25622 are I2C-controlled single-cell chargers with NVDC Power Path Management, Integrated ADC, and OTG Output.
For detailed features and operation, see Table 1-1 table for a list of devices and their data sheets.
This EVM supports the following features:
This EVM does not include the EV2400 or USB2ANY interface boards. To evaluate the EVM, an EV2400 or USB2ANY must be ordered separately.