SLUUCQ0A may 2023 – june 2023 TPS922052 , TPS922053 , TPS922054 , TPS922055
Figure 5-1 shows the efficiency versus input duty cycle in analog dimming mode. The full-scale LED current IFS is set at 4 A. The frequency of the input PWM signal at the ADIM/HD pin is 20 kHz. Input voltage VIN is 48 V. The load is 8 white LEDs in series.
Figure 5-2 shows the efficiency versus input duty cycle in PWM dimming mode. The full-scale LED current IFS is set at 4 A. The frequency of the input PWM signal at the PWM/EN pin is 20 kHz. Input voltage VIN is 48 V. The load is 8 white LEDs in series.