SLUUCR2 October 2023 TPSM843620
The TPSM843620EVM is provided with input connectors, output connectors, and test points as shown in Table 3-1 and Table 3-2.
To support the minimum input voltage with the full rated load on both outputs with the default EVM, a power supply capable of supplying greater than 5 A must be connected to J2 through a pair of 20-AWG wires or better.
For U1 the load must be connected to J1. A pair of 20-AWG wires or better must be used for each connection. With the maximum current limit setting, the maximum load current capability is near 8 A before the TPSM843620 goes into current limit. Wire lengths must be minimized to reduce losses in the wires.
TP3 provides a place to monitor the VIN input voltage with TP4 providing a convenient ground reference. TP9 is used to monitor the output voltage of U1 with TP10 as the ground reference.
If modifications are made to the TPSM843620EVM, then the input current can change. The input power supply and wires connecting the EVM to the power supply must be rated for the input current.
For the FSEL pin of the TPSM843x20 to correctly detect the resistor value connected to ground, the buffers on the EVM need to be provided a VCC voltage of 2 V to 5.5 V to go high impedance. Populating the shunt on J3 enables the output of the buffer.
REFERENCE DESIGNATOR | NAME | FUNCTION |
---|---|---|
J1 | VOUT | VOUT screw terminal to connect load to output. |
J2 | VIN | VIN screw terminal to connect power to input. |
J3 | EXT SYNC | 2-pin header to connect U2 buffer output enable to ground. Populate shunt to enable output of buffer. Remove shunt to make buffer output high impedance. |
J4 | MODE | MODE selection header. Use shunt to select MODE resistor. See Table 2-3. |
J5 | SYNC/FSEL | FSEL selection header. Use shunt to select FSEL resistor. See Table 2-2. |
REFERENCE DESIGNATOR | NAME | FUNCTION |
---|---|---|
TP1 | VIN | VIN test point. Use this for input ripple measurements. |
TP2 | PGND | PGND test point. Use this for input ripple measurements. |
TP3 | VIN_EFF | VIN test point near input terminals. Use this for efficiency measurements. |
TP4 | PGND_EFF | PGND test point near input terminals. Use this for efficiency measurements. |
TP5 | PGOOD | PGOOD test point. |
TP6 | AGND | AGND test point. |
TP7 | VOUT | VOUT test point. Use this for output ripple measurements. |
TP8 | PGND | PGND test point. Use this for output ripple measurements. |
TP9 |
VOUT_EFF |
VOUT test point near output terminals. Use this for efficiency measurements. |
TP10 | PGND_EFF | PGND test point near output terminals. Use this for efficiency measurements. |
TP11 | EN | EN test point. If applying an external voltage, then EN must be kept below the absolute maximum voltage of the EN pin of 6 V. |
TP12 | VOUT | meSMB connector to measure output voltage. When using this test point, make sure the scope is set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP13 | EXT_SYNC | SYNC test point. Supply an external clock to this test point if using one. |
TP14 | SYNC/FSEL | FSEL test point. |
TP15 | MODE | MODE test point. |
TP16 | BODE | Test point between voltage divider network and output voltage. Used for Bode plot measurements. |