SLUUCS5A january 2023 – july 2023 UCC14141-Q1
The UCC14141-Q1 is the default IC used in the UCC14141EVM-068 but any of the alternate versions listed in Table 1-1 can be used for evaluation. Each of the component versions listed in Table 1-1 are pin-to-pin compatible, functionally equivalent, drop in replacements with respect to one another. Component part numbers beginning with “P” indicate pre-production material but are the same IC as “non-P” marked components.
General Part Number | Orderable Part Number | Isolation/Surge/Working Voltage |
---|---|---|
UCC14141-Q1 | UCC14141QDWNQ1 | 5 kVRMS/10 kVPK/1 kVRMS |
PUCC14141-Q1 | PUCC14141QDWNQ1 | 5 kVRMS/10 kVPK/1 kVRMS |
UCC14140-Q1 | UCC14140QDWNQ1 | 3 kVRMS/6.5 kVPK/850 kVRMS |
PUCC14140-Q1 | PUCC14140QDWNQ1 | 3 kVRMS/6.5 kVPK/850 kVRMS |
If U1 replacement is required, then TI recommends to always use best practice soldering techniques. Techniques can include taking appropriate ESD precautions and having qualified personnel, skilled at surface mount soldering and board level rework, removing and installing U1. Visually verify the desired UCC1414x-Q1 component version is properly installed in the EVM. If rework on U1 has previously been performed, then visually verify correct orientation of U1 according to Figure 1-1. The pin 1 identifying dot on top of the IC package is oriented at the top left according to Figure 1-1.