Use the following instructions to verify state transition of TPS12130-Q1 through load wakeup trigger
- Apply 12 V at the input of the EVM at no-load.
- Enable the EN/UVLO to HIGH.
- Now, gradually increase the load current from 5 mA to 200 mA and observe the
transition from low power mode to Active mode at the pins of G1 (TP5), G2 (TP1),
WAKE (TP13) and load current using oscilloscope.